• ADG5433/34: undesirable Vdd voltage while floating

    Hi,

    I have a ADG5433 witch on my circuit. Unfortunatley there is a situation when the following configuration is occuring due to the design.

    Condition:  Vss and Vdd floating, Pin 16 (GND) to circuit GROUND.

    And IN1, IN2 And IN3 (pin # 8, 9, 15) to…

  • EN pin/Output pin of ADG5433

    Hi


    Please let me ask 2 questions about EN pin/Output pin of ADG5433.

    Can I think EN pin output gets High-Impedance when EN pin is set High ?

    And during disabling output, should output pin be under max absolute rating when other voltage level is…

  • ADG5433 generates voltage spike at output while switching at 100KHz

    Hi All,

    I have used Analog switch to generate 100KHZ square with variable voltage range from 1V to 15V.

    While generating square wave, i am getting voltage spikes on both falling/rising edge which i have tried RC filter to remove at output of analog…

  • pspice model for ADG5412/ADG5413 or ADG5433/ADG5434?

    Sir:

         Is there pspice model for ADG5412/ADG5413 or ADG5433/ADG5434? I am designing a project and need a switch that can drive output voltage as large as 30V. I want to use these switches to do a simulation first.

    Thank you !

    Best wishes

    Jacky 2012…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • 问题: ADI最新中文资料(2011年6月)

  • RE: Problem with ADG1606 protection

    Hi imanjohn,

    Have you any more details on what the fault is that is damaging the part? Is it a positive or negative over voltage condition?

    I have attached a tutorial which outlines protection methods to be used. You have implemented one of them but…