Hi Gerd,
Unfortunately we do not have a SPDT device in a MSOP package with an enable pin.
As you have said, this is to maintain compatibility with legacy devices.
At the moment there are no plans to release an MSOP version with an enable pin but your…
Hi.Are you planning to connect ADG5419 at the output channels of AD9106?If yes, then please add the series resistance of ADG5419 in matching the impedance at the primary side and secondary side of the RF transformer connected to AD9106 outputs.For example…
Hi,
Pin 5 in the ADG5419 is not internally connected so 5V could be presented to pin 5 of the ADG5419.
Regards,
Stephen
I am looking for a PSPICE model of ADG5419. Is there a comparable part that can be used instead?
I used ADG5419 to output a very weak ultrasonic echo signal, which cannot be observed with an oscilloscope. Is there any corresponding solution to amplify the signal? If it can be directly amplified, it will be better to process the imaging.Is there any…
我使用adg5419,ADA4899产品作为超声解决方案,采集回来的信号是电信号,请问有没有下一步的产品将电信号处理为图像信号?
HI Lorenzo,
Yes the ADG1408 and the ADG1419 are based on the same technology.
The ADG5419 has an internal VL generator that is used to power the input buffer at a lower voltage so you can use a lower digital logic voltage without significantly impacting…
Hi Kenny,
It is possible that you are triggering a latch-up event. You could try to prevent this by putting a schottky diode from Vss to Ground to prevent Vss going 0.7v above Ground. Alternatively you could look at the ADG5419 Latch up immune version…