• RE: Short to Battery Protection Circutiry for Automotive Video Decoder

    Hi Theresa,

    Thanks so much for getting back to me.

    The solution you have proposed looks really good. Do you mind if I describe the setup and how I think the circuit will work. Is the below correct?

    Setup:

    Use an ADG5413F.

    Set Vdd to +5V. Set VSS…

  • RE: Alternate IC for ADG1434 with power off protection

    Hello Suresha,

    Unfortunately, we do not have a QUAD SPDT with power off protection in our portfolio.

    The newly released ADG5413F has a higher voltage span than the ADG4612 and can be used in an SPDT configuration. Each ADG5413F can be configured as…

  • ADG5413 high impedance

    Hi,

    Is it allowed to supply the ADG5413 with 5V when all switches only have to remain open (high impedance)?

    During this device state the inputs off the ADG5413 will be 2.5V +- 0.3V

    When the ADG5413 is switching, it's supply will be >=9V (Minimal listed…

  • RE: ADG1213 max digital IN voltage at power down

    Hi,

    You are correct the max IN voltage we would recommend during power down is 0.3 V. This is due to the protection diodes on the input.

    You could have a look at the ADG5413F, this device has power off protection on the source pins and the digital inputs…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • FAQ: ADG54xxF

    Q1. Can you explain the Fault detection function to me and how it may offer benefits to my system?
    A1. The voltages on the source inputs of the ADG5412F are continuously monitored and the state of the switch is indicated by an active low digital output…

  • 最新中文资料更新20150610

  • 微信焦点(第1期):匆匆这一年——回顾ADI精彩2014

    这一年,一家非常牛的微波技术公司——HITTITE归入ADI旗下

    Hittite在RF、微波和毫米波技术方面的优势,对ADI在RF和信号转换方面的雄厚实力形成了良好补充。借助两家公司的合力,ADI将为客户打造更加全面的解决方案,拓宽在工业、通信基础设施和汽车市场的疆土。不久前,ADI正式宣布其全球分销网络提供Hittite微波产品。

     

    这一年,ADI收获很多荣誉

    ADI被评为美国最环保企业50强


    在《新闻周刊》2014年美国环保企业排名中…

  • 微信焦点(第1期):匆匆这一年——回顾ADI精彩2014

    微信焦点(第1期):匆匆这一年——回顾ADI精彩2014 by ADI_Amy

    这一年,一家非常牛的微波技术公司——HITTITE归入ADI旗下

    Hittite在RF、微波和毫米波技术方面的优势,对ADI在RF和信号转换方面的雄厚实力形成了良好补充。借助两家公司的合力,ADI将为客户打造更加全面的解决方案,拓宽在工业、通信基础设施和汽车市场的疆土。不久前,ADI正式宣布其全球分销网络提供Hittite微波产品。

     

    这一年,ADI收获很多荣誉