• ADG5413 high impedance

    Hi,

    Is it allowed to supply the ADG5413 with 5V when all switches only have to remain open (high impedance)?

    During this device state the inputs off the ADG5413 will be 2.5V +- 0.3V

    When the ADG5413 is switching, it's supply will be >=9V (Minimal listed…

  • pspice model for ADG5412/ADG5413 or ADG5433/ADG5434?

    Sir:

         Is there pspice model for ADG5412/ADG5413 or ADG5433/ADG5434? I am designing a project and need a switch that can drive output voltage as large as 30V. I want to use these switches to do a simulation first.

    Thank you !

    Best wishes

    Jacky 2012…

  • MAX14763ETA+ alternative

    I'm search equivalent from an maxim  spdt analog switch The MAX14763ETA+ i use
    this parts for Can Bus Termination and for pull-up resistor on automotive
    diagnostic in a range from 12-24V have you an equivalent parts for this?

     

    The Maxim part…

  • ADG5413BRUZ无法关断

    ADG5413BRUZ在单电源24V供电时,控制引脚 INx 用 5V 的 I/O 控制,IN1与IN2短接,用一个I/O控制,在高电平时S1通道导通,S2通道处于半导通状态,即导通电阻15K左右,在低电平时S2完全导通,S1也完全导通,是什么原因导致的呢?求解答!

  • RE: ADG1412 - When IN signal is Logic "1" the switch is activated meaning closed. The data sheet says S and D terminals could both be Input/Output. Does this mean S and D are shore circuited when IN is logic 1 ?

    David,

    I understand that the Voltage across the S/D terminals cannot exceed Vdd - Vss.

    This is tricky because the ADG14xx is a switch, when it is ON behaves like a wire but in the range of Vdd-Vss.

    Looks like we have to use ADG5412/ADG5413 for higher…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • 问题: ADI最新中文资料(2011年4月)

  • RE: Problem with ADG1606 protection

    Hi imanjohn,

    Have you any more details on what the fault is that is damaging the part? Is it a positive or negative over voltage condition?

    I have attached a tutorial which outlines protection methods to be used. You have implemented one of them but…