Hello,
I'm using ADG5408 8:1 mux which has 28Vdc/Open discrete input. We are using 28Vdc for Vdd of the mux and other condition is as below.
- EN: 3.3V, A0~A1: 3.3V
- Vss: GND and connected to exposed pad
- S1~S8: 28Vdc/Open discrete input
Hello ADI,
The ADG5408 is a high voltage analog multiplexer. I want to understand if there is a minimum voltage specification for the device. I will run the device in bipolar mode, and I'd like to go below the +/-9VDC the datasheet seems to say in can…
I have a question about the supply voltage of the ADG5408. I would like to use for VDD a Supply of 38V and for VSS -3.3V. Unfortunately, the VDD to VSS voltage isn't described in the datasheet only the absolute maximum Ratings. What is the…
I was wondering what the power dissipation thru the device is.
What about the leakage current in this circuit, leaking current from drain to source, or from the Vs to the source?
Specific example.
Vss +16V Vdd - 16V
On Drain 0- +15V
On source S1 - S8 switched resistors for current measurement, voltage drop across…
Hi
Could you please let me know how much the maximum voltage level of Source terminal pins of ADG5408 during power off ?
Regards,
Hiroyuki
I have a question about the supply voltage of the ADG5408. I would like to use for VDD a Supply of 5V and for VSS -24V.
Does this connection violate the description below?
Thank you.
For the ADG5206, ADG5208, or ADG5408 multiplexer, what is the current consumption when the digital input is around 3V, and not around Vdd?
I need +/-12V as the power supply of the multiplexer.
Vinson
hellow
In some ic ADG5408 28/open gnd/open ,Does it mean the end is powered from some board and grounded in ADG5408
regards
AGXIN.J
I just found the ADG5408, which appears to be a better choice.