• ADG5404F switch noise

    I'm using the ADG5404F. When I switch the addree A1 and A0, A 5V pulse of approximately 400ns long appears at the D port. This has a serious impact on my system. Is there any solution to remove it? The VDD is 8V. The VSS is -8V. There is 32 adg5404F…

  • Using ADG5404F mux like a demux?


    Hi All,

    We would like to use ADG5404F multiplexers to select output for a single current source. I am wondering if it is possible to connect the current source to the D pin (pin 6) and sink on the S pins (pin 4,5,10,11) with using 40V single power supply…

  • ADG5404 Current

    Hi, 

       I am using ADG5404F as Multiplexer, but encounters several questions. 

      1) In my application, 100~200mA continuous current is needed, is ADG5404F ok?

      2) I check the datasheet, it mentions continuous current up to 280mA(Table 5), but in ABSOLUTE…

  • RE: analog multiplexers without Power Off Protection

    Hi,

    When the ADG5408 is un-powered the device will be in an undetermined state.

    The ADG5404F is a 4:1 Mux with fault protection.

    Can you share your application and I would be glad to review and recommend a switch selection.

    Regards,

    David

  • RE: Multiple Channels with AD4110-1

    Hi,

    Apologies for the delay. The system would require a fault protected switches/muxes such as ADG5404F(4:1 mux) However, for 18 channels this will require around 15xADG5404 for example since there are 3 pins to switch in, V+, V- and RTD pins.

    I would…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • FAQ: ADG54xxF

    Q1. Can you explain the Fault detection function to me and how it may offer benefits to my system?
    A1. The voltages on the source inputs of the ADG5412F are continuously monitored and the state of the switch is indicated by an active low digital output…

  • RE: Looking for relay replacement IC

    Hi,

    You could take a look at the ADG5404F it is a 4:1 Multiplexer. it has a maximum single supply voltage of 44V or +/-22 V Dual Supply. The multiplexer also has input overvoltage protection up to +/-55 V.

    For more information on this part and our overvoltage…

  • 最新ADI官方中文技术资料更新 (2015年4月)

  • RE: Audio switch

    HI Teodor,

    Thanks for the clarification,

    For the single SPST request have a look at the ADG1401. Very low Ron & Ron flatness and this is available in a 8-Lead MSOP or 8 LEAD LFCSP package.

    Details here: http://www.analog.com/media/en/technical…