Hi,
Thanks for getting in touch.
The ADG5243F is an triple SPDT switch. however the maximum operating voltage is 44 V.
Can you share more details about your application and why you require up to 46 V?
Regards,
David
最近我在项目上采用了AD7124-4芯片进行PT100温度传感器采集温度,采集效果还不错,采用比例测量法。外部用ADG1607模拟开关来进行通道切换。
但是我看ADI给的参考设计都是AD7124的PIN管教直接连接PT100传感器,我的设备传感器连接线缆超过1米,因此我担心ESD干扰或者其他的信号对AD7124
造成损坏,我看一般的建议是加限流电阻、TVS和ADG5243F进行保护,但是ADG5243F成本太高了,不知道还有没有其他的方法对AD7124进行保护呢?
Hi David,
At first flance, the ADG5243F looked good for our application.
Unfortunately, we needed to use the switch in a SPDT configuration (with
the high voltage on the SP side), so this IC does not fit.
In the end we have completely changed the…
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |
Hi Mark,
Apologies for the delay, See below for the ADG5243F
Θjb = 16.67°C/W
Rjc for exposed paddle packages is normally measured to the exposed paddle.
However where Rjc is to be used as part of a 2 resistor compact thermal model/simulation, then…
Q1. What are the key benefits of these fault protected switches?
A1. There are a number of key features on these parts
ADI 中国技术支持中心为客户整理了“开关与多路复用器产品常见问题解答_Rev 2.1”,其在原有“开关及多路复用器产品常见问题解答 Rev 1.0”的基础上进行了补充升级,供客户自助快速查询常见问题的解决方案。PDF