• RE: ADG5208 - connecting outputs together on multiple devices

    Hi Bill,

    That is an acceptable use case. Below is a link to an article dealing with multiplexing data acquisition signal chains and a link to a circuit note that uses the ADG5208 for signal chain multiplexing.

    https://www.analog.com/en/analog-dialogue…

  • ADG5208: THD specifications missing at the ADG520x family

    For Hi-Fi Audio, THD is an important figure and I am looking for a device
    ideally with a maximum THD of 0.002% THD+N across the 20Hz - 20kHz frequency
    range.  Can you please advise whether this information is available for any of
    these…
  • ADG5206, ADG5208, or ADG5408 current consumption

    Hello,

    For the ADG5206, ADG5208, or ADG5408 multiplexer, what is the current consumption when the digital input is around 3V, and not around Vdd?

    I need +/-12V as the power supply of the multiplexer.

    Vinson

  • RE: ADG2188多颗串联信号带宽评估

    你好,

    开关串并联之后都会影响信号带宽,你需要从寄生电容和导通阻抗两方面考虑。并联的时候,带宽受电容的影响较大,串联的时候带宽受电阻的影响较大。举个例子,对比ADG5208和ADG5209两颗芯片,ADG5208是8:1,ADG5209是4:1,也就是说ADG5208并联的通道数量是ADG5209的一倍,从数据手册可以看出ADG5208的带宽减小到了ADG5209的一半左右。

  • Are these parts pin-pin compatible with existing parts?

    Are these parts pin-pin compatible with existing parts?

     

    Yes, the ADG5208F/ADG5209F are pin-for-pin compatible with the ADG5208/ADG5209
    and ADG1208/ADG1209. They are drop in replacements if overvoltage protection is
    required. However…
  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • 热门器件推荐,你需要哪款?

    我们根据客户不断变化的设计需求,定期更新官网的IC产品,并在论坛上推荐给您。本月主打的产品包括:

    运算放大器ADA4622

    http://www.analog.com/cn/products/amplifiers/operational-amplifiers/ada4622-2.html

    ADA4622-2是新一代AD822单电源、轨到轨输出(RRO)、精密JFET输入运算放大器。ADA4622-2包括许多使其成为理想升级版本的改进,且灵活性和易用性不受影响,这使AD822非常适合各种应用…

  • RE: ADG1208 power supply sequencing

    Hi HM,

    The best power up sequence for the ADG1208 is:

    1. Vss
    2. Ground
    3. Vdd
    4. Digital
    5. Source/Drain

    While the maximum ratings show 35V as the largest voltage allowed between Vdd and Vss it is not recommended to operate the part with this level of…

  • FAQ: ADG52xxF

    Q1. What are the key benefits of these fault protected switches?

    A1.  There are a number of key features on these parts

    • Overvoltage fault protection to +/-55V levels in powered and unpowered state
    • Secondary supply rails to allow for user defined…
  • 重磅推荐!ADI 体外化学分析仪解决方案

    最新解决方案已上线,点击:http://h.analog.com/CN-VC-ANALYZER-ff?ADICID=SOME_CN_P114971 下载完整文档

    体外化学分析仪的典型架构

    生命科学与医疗仪器仪表包括各种不同的系统,比如体外化学 分析仪、流式细胞分析仪、输液泵、透析设备、呼吸器、导管 等设备。体外化学分析仪利用许多电化学和光学技术来分析血 液、尿液、脑脊髓液和其他生物学样本。其中使用最广泛的技 术是光学测量,实例包括比色、吸收、光谱测定和荧光检测方 法。可通过这些方式测量体液中的抗原…