• ADG507A multiplexer ground

    Hi,

    I'm working with the ADG507A Multiplexer. I currently have it set according to the schematic:

    The output goes to an AD595 Thermocouple Amplifier, and the input connects to a grounded thermocouple. The AD595 requires a connection to ground from…

  • ADG507A Max Enable Voltage

    Hi,

    I'm working on using the ADG707A Multiplexer with the AD595 Thermocouple amplifier to build a thermocouple multiplexer. I am basing it off of the thermocouple multiplexer in the application notes (AN-369). I notice that you suggest permanently enabling…

  • ADG507A with AD 8497 thermocouple ampr

    Helo all,

    I am a research fellow, Doing work in mechanical engineering, In my experiment i want to measure the temperature from 12 different points using T type thermocouple with the surrounding atmosphere conditions are between 25-100 degree centigrade…

  • RE: adg507 voltage driving

    Hi Aliakbar,

    VDD = 5V for the ADG507A is okay. However, there is no specification table for this voltage so specs cannot be guaranteed.

    If guaranteed specifications are need then the ADG707 would be a good alternative as it has a full specifications table…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • Analog MUX - Absolute max I/O differential with enable off

    Hi, I am an EE working on a battery monitoring system for the Electric Motorcycle Project at an undergraduate college and was looking at the 8 channel differential analog multiplexers (ADG1407, ADG507A, ADG509A, ADG5207). Could anyone tell me the max…

  • AD595: Why are there two different operating temperatures listed in datasheet for the same part number?

    In the absolute max rating section of the AD595 datasheet, you quote the
    operating
    temp range as being -55 to +125. However, in the second sentence of the fifth
    paragraph of the Product Description on Page 1 of the datasheet you state 'Both …