• ADG4612 Failure mechanism

    I am interested to know what happens when an ADG4612 fails. Does it fail short, open, shorts to ground, etc..?

    I would like to connect the drains of two switches (two different packages) to the same net and only power one devices at a time. The power…

  • RE: Regarding ADG4612

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: the question about the ADG4612

    Hi,

    Apologies for the delayed response to your query.

    These components that you are asking about are not actually mounted on the evaluation board. We have left space for users to add their own resistors and capacitors if required in their signal chain…

  • ADG4612输入范围

    我有一个关于模拟开关数据手册的问题。

    最大导通电阻平坦度指的是什么?它与导通电阻有何区别?

    期待您尽早回复。

  • ADG4612

    I'd like to get a better understanding of the noise and distortion properties of the ADG4612 part.  This is a 4:1 analog MUX rated at a bandwidth of 193 MHz, but the data sheet treats it as an audio part, with the THD+N characterized with an AP audio…

  • Does ADG4612 have latch-up immune feature ?

    Hello,

    I have a question about ADG4612.

    In the selection table of below URL, ADG4612 has latch-up immune feature.

    http://www.analog.com/en/products/switches-multiplexers/latch-up-immune-high-esd.html

    But in the datasheet(Rev.9) , it is not described…

  • How fast can ADG4612 can turn on and off

    Hi,

      I would like to know how fast the ADG4612 can turn on and off? What happend if 1MHz clock is feed into the INx pin?

    Thank you,

    Khai.

  • ADG4612 output problem

    Dear Madam/Sir,

    I am using the ADG4612 switch in my design. I connect Vdd to 3.3v and Vss to 0v

    However I am getting false outputs in those two cases:

    - when enable is off and Vin > Vdd+Vt I get an output equal to Vin/2 while i should get nothing…

  • ADG4612 isolation mode to normal mode conditon

    Hello.

    I have questions about ADG4612.

    I experimented in the order of 1, 2.

    1 VDD Power off and input signal to VS(5V TTL 10 MHz).

    2 And then. VDD supplied 5V ,VSS was GND and VS continued input signal.

    In 2 of the conditions, AD4612 was supposed…

  • ADG4612 isolation mode negative condition failed after two power up

    Hello,

    I use a ADG4612 with 0V on GND pin and Vss pin, and +8V on Vdd pin for the on condition. All INx are connected to +8V also at the same time on power up.

    Initial step : (power supply OFF) Vdd floating ,INx floating. and Dx floating

    Second step…