• ADG444 : typical supply current and maximum supply current

    Hello,

    I have a question about supply current of ADG444 from our customer.

    Typical specification of IDD and ISS under 25'C is 0.001uA and maximum it is 1uA.
    It is 1000:1 ratio between typical value and maximum value at same temperature.
    I can't imagine…

  • ADG444 are used at mountains

    My customers want to use parts(ADG441BRZ) at high altitude.
    Are parts affected by atmospheric pressure when parts are used at mountains with altitude 1000m to 3000m?
    I read the Reliability Handbook(UG-311), but I could not find the corresponding article…

  • ADG444 VL pin input voltage

    Hello,

    I got a question about VL pin voltage on ADG444.

    Some customer would like to use this ADG444 in +\- 15V supply environment.

    At this time, can VL pin be connect +15V(VDD)?

    According to the topic as below,

    http://ez.analog.com/message/3255…

  • ADG441/442 and VL pin

    On the ADG441/2 devices pin 12 is an NC pin.  On the ADG444 it's required to be connected to +5V.  ADG441/2 have a lower resistance cousin, the ADG451/2 parts; I use either, depending on needs.  Well... in these days of parts shortages, I may need to…

  • AD7843 are used at mountains

    My customers want to use parts(AD7843ARQZ) at high altitude.
    Are parts affected by atmospheric pressure when parts are used at mountains with altitude 1000m to 3000m?
    I read the Reliability Handbook(UG-311), but I could not find the corresponding article…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • ADG442: low logic level clamped to about -1V.

    In my prototype, ADG442 is not  The problem seems to be that the digital inputs
    are driven with +15V and -15V logic levels, but the ADG442s are clamping the
    low logic level to about -1V. The data sheet (rev. A, 2005) gives the maximum