• ADG411 Usage

    Hello, just a quick one, what is the normal operation temperature of the ADG411 component with a power rail +/- 12V?
    Explanation, I have a device (which is down) that uses 2 of these components. The first heater at about 94°C and the other at 58°C.…

  • ADG411: logic threshold voltage over digital supply.

    Would you please help to understand the the typical expected threshold voltage
    as a function of digital supply voltage, VL.

     

    Please see the attached application note for the ADG451 VL voltage threshold.
    The ADG411 has a similar logic…
  • ADG411: is ist possible to worf with a 3V Logic Level?

    I want to use the ADG411 +-12V but with a Vlogic=3V - would this work?

     

    Yes it is possible to apply 3V to the Vl pin. We just have it specified at 5V.
    For the ADG412 the Vl applied can be in the range of -0.3V to Vdd +0.3V.  Our
    parts…
  • Question about ADG1211

    Hi All,

    Can  I use 15V/0V for INx pins (Logic Control Input pins) under VDD=15V and VSS=-15V conditions?

    Also, ADG411 and ADG1411 can be used same conditions?

    Best Regards,

    Kazu

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • RE: Need spice model for ADG419

    Hi,

    There is no spice model available for the ADG419.

    One option is to use the ADG411 Spice model.  The ADG411 is 4 xSPST so you can use 2 channels and tie the outputs together to replicate an SPDT.  The ADG411 has the same core switch design as the ADG419…

  • RE: ADG5404 cross talk?

    Hi Nico,

    Initially looking at your plots what comes to mind is switch charge injection effects.  I have attached an FAQ that has some Q&A on glitches caused by charge injection.  An experiment to do would be to increase the shunt capacitance on the…