• ADG333A switching frequency / bandwidth information?

    For the ADG333A switch, our intended signal is 500 KHz sine wave input. What is
    the bandwidth of this device?

     

    We don’t have any bandwidth information for this part. However, the bandwidth
    will be well in excess of 500kHz.
    As some…
  • ADG333A POWER SUPPLY SEQUENCE

     About ADG333A ,  turn on VSS  first, followed by VDD,  and VDD-VSS not exceed +44 V, I want to know there is a problem?

  • ADG333A POWER SUPPLY SEQUENCE

    About ADG333A , turn on VSS  first, followed by VDD (opposite of recommendation),and VDD-VSS not exceed +44 V,I want to know there is a problem?

  • What is risetime or falltime of the ADG333A?

    According to the ADG33A datasheet I know the switch time information is as show below, but I want to know the switch signal  VS from 10%-90% rise or fall time, can you help me?

  • offset voltage problem with analog switch ADG333A, pin-compatible substitute?

    Hello,

    I've got offset voltages of 0,2V with a device containing ADG333ABNZ. Do the pin compatible newer versions like ADG1434 or ADG5434 correct this?

    Best regards,

    Simon Brem

  • Can the ADG333 be powered from a single 24V supply?

    Can the ADG333 be powered from a single 24V supply?

     

    Yes ADG333A can be powered from a single 24V supply. VSS should be connected to
    GND when operating with a single supply. See also section on ADG33A supply
    voltages and Power Sequencing…
  • ADG333A_Status_WhenInputFloat

    One ADG333A's question need your verification.
    When the IN Pins are float, then what status of the switch? The D is switched
    to S1A or S1B?

     

    We cannot guarantee the status of the switch when the IN pins are floating.
    Internally…
  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225