Hi VPANDEY482,
Yes. You can connect devices with an open-drain output configuration to ADG3300 to bi-directionally translate certain voltage levels through the Vcca and Vccb supplies.
Best Regards,
Christian
Hi VPANDEY482,
Yes. You can connect devices with an open-drain output configuration to ADG3300 to bi-directionally translate certain voltage levels through the Vcca and Vccb supplies.
Best Regards,
Christian
I'm trying to use the ADG3300 to simply translate between a 3.3V and a 5V system . Originally I had planned to
use the auto-sense capability for bidirectional signals,but have decided the part is way too unstable for that to ever work.
Is it possible…
Hi~
I designed the circuit as shown below.
State
- If the FPGA outputs a high signal, the input(@ADG3300) will oscillate.
- But without the ADG3300, no vibration will occur.
- If the FPGA outputs a low signal, both the input and the output (@ADG3300…
Hi,
I am trying to find a simple 1.2V to 5V CMOS-CMOS level translator. I was looking at the the ADG3300 but realized that the datasheet states that the input must be driven by a low impedance output (less than 150 ohms). Just wondering where is the…
Dear Expert,
I checked the level-shift ADG3300/3308 datasheet, which can't showed any information of Minimum Pulse Width /Pulse duration specification, Can you help? Thanks you!
Hi all,
I am using the ADG3300 level translator to interface an FPGA output (3.3V signal , 1MHz frequency) to an IC working at 1.8V. I get severe oscillations of 50 MHz at the output. I have used all the good PCB practices like good decoupling , ground…
Hello,
we need to interface the AD7124-8 with an ATMEGA32U4 (5V mcu) through SPI. We are conisdering the attached shifting diagram:
Does anybody have any insight on:
1. Will we have any issues with the fact that we are not using any pull-ups particularly…
Hi Moto,
I found an 8 channel bi directional level translator that I hope you can use for the interface on your application. Please check on the ADG3300. ( please refer to link ADG3300 datasheet). You may also want to do a parametric search on other…