Q
We would like to know the number of logic gates / transistors used in ADG3248
Hi everyone,
I am trying to build a FSK modulator for a 10Mbps data rate. The idea was to use 2 Oscillators ~50MHz connected to a Switch capable of selecting one of the two inputs at that 10MHz rate. Is ADG3248 Capable of doing that?
Thank you
Hi Mohammad,
Unfortunately, the ADG3248 does not cover this wide range and negative level translation.
I would think the level translation you need can be catered by using operational amplifiers.
Best Regards,
May
The ADG324x family are level translators that is capable of translating voltage levels from high to low only. This statement can be supported by the Truth Tables and is further discussed at the Mixed Voltage Operation, Level Translation Section of the…
FAQ: How to achieve the level translation in ADG324x switches?
Answer:
The signal applied to either the A or B pins of the ADG324x family of bus switches is clamped at the maximum pass voltage level specified in the datasheet. The maximum pass voltage is…
FAQ: What is the meaning of the “Maximum Pass Voltage” specification listed in the datasheet of the ADG324x bus switches?
Answer:
The maximum pass voltage specification on the ADG324x family of bus switches represents the maximum voltage that…
FAQ: Can I use ADG330x for I2C applications?
Answer:
The ADG330x is not recommended for I2C applications. The ADG330x architecture shown in the Theory of Operation section of the datasheet uses an internal resistor to ensure the device operates correctly…
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |
Can you please explain the meaning of the "Maximum Pass Voltage" specification listed in the datasheet for the ADG324x bus switches?
The maximum pass voltage specification on the ADG324x family of bus switches represents the maximum voltage…
How is the level translation achieved with the ADG324x bus switches?