• ADG3246 3.3V-to-1.8V Translation Not Working

    Hi,

    I am using the AD3246 to level translate a unidirectional bus from 3.3V down to 1.8V.  The bus runs at 150 MHz.  The device is physically placed in the middle of the bus.

    I have connected BEn to ground, SELn to ground, VCC to 3.3V.

    My problem is…

  • ADG3246 IO driver current or sink current max.

    Hello,

    May I know how many ADG3246 IO driver current output or sink current input max?

    I wil try to use ADG3246 between FPGA and SATA singal level translator, and also do LED driver for status show up.

  • RE: Bus Enable on ADG chips

    Hi May,

    I've been looking at the ADG3247 and ADG3246 parts primarily.

    Thanks,

    Zach

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • ADG324x Level Translation: high to low

    The ADG324x family are level translators that is capable of translating voltage levels from high to low only. This statement can be supported by the Truth Tables and is further discussed at the Mixed Voltage Operation, Level Translation Section of the…

  • Maximum Pass Voltage on the ADG324x bus switches

    Can you please explain the meaning of the "Maximum Pass Voltage" specification listed in the datasheet for the ADG324x bus switches?

    The maximum pass voltage specification on the ADG324x family of bus switches represents the maximum voltage…

  • Level translation with ADG324x bus switches

    How is the level translation achieved with the ADG324x bus switches?

  • Maximum Pass Voltage on the ADG324x bus switches

    Can you please explain the meaning of the "Maximum Pass Voltage" specification listed in the datasheet for the ADG324x bus switches?