• ADG3123 analog voltage range

    To whom it may concern, 

    I am intrigued by the ADG3123 because it affords logic-level to high-voltage bipolar outputs. However, I do not necessarily need the high voltage range specified in the part datasheet. Can this part operate at VDDA=VDDB=3V or VDDA…

  • ADG3123 Output signal swing

    What is the maximum achievable output signal swing on the ADG3123?

  • ADG3123 Slew Rate

    Dear All:

    ADG3123 Spec. is show Rise/fall time: 12 ns/19.5 ns typical & Operating frequency: 100 kHz typical but not show Slew Rate parameter ,can you tell me this parameter spec. thanks

    Best

    Jack

  • Level Shifting from 5V to 24V with ADG3123?

    For an interface from standard 5V logic to industrial field bus adapters with 24V logic I would like to design a compact 16 channel level shifter with active drivers on the 24V side (5V input to 24V output).

    I found the ADG3123 chip which seems to focus…

  • Looking for a bigger package version of ADG3123

    I have a project where I am trying to take a 3.3V GPIO pin out of an SoC (Raspberry Pi to be exact) and use it to drive a control input that wants to be >= 15V. I found teh ADG3123 which fits the job nicely, the only problem I have is I am trying to breadboard…

  • RE: Level Translator ADG 3123

    Hi Chunya,

    I moved your question on the ADG3123 to the Switches/Multiplexers community. Someone here should be able to assist you.

    Thanks,

    Kris

  • AD8112 - Is it possible to work with 3.3V Digital Supply?

    I need more information about the digital Supply Voltage of the AD8112.
    Which is the operating voltage of the digital part?
    Can I use a 3.3 volt digital power supply?
    If the the analog supply is +-5Volt and the digital supply is +5V, can…
  • RE: ADG3123BRUZ level shifter

    Hi Stathej,

    No, the ADG3123 does not have pull down/up resistors on its input and the maximum frequency is up to 100 kHz (for capacitive loads = 100pF).

    Take note that in order to operate the device properly, digital input conditions must be met. For…

  • RE: Need a High Voltage Level Translator

    Hello YSVenu,

    The ADG3123 is the only High Voltage level translator that we have.

    I believe that it is possible to use this part in the manner you have described above, but we have not tested it with inputs above 5.5V and don't have any information…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225