• Can i use AVDD =5V0,AVSS=0, in ADG2128?


    Hi,

    In my application i am using ADG2128, can i give vdd=5v0 and vss=0.

    In datasheet there is only two option 12v0 single supply and +-5v0 dual supply,

    Instead of 12v0 if we give 5V0 whats the difference?

    Thankyou,

    Sony Sunny.

  • ADG2128 Output stage ( Hi, Lo, Hi Z) of the I/O when the switch is off

    I wonder if you could help me to know what is the state ( Hi, Lo, Hi Z) of the
    I/O when the switch is off.

     

    The off Isiloation is -69db.

    This means if you have a 1V Signal at the Input you will see 385uV Signal at
    the output.
  • RE: AD2128 problem with audio breaking through open switches

    Hello Tim,

    If you are not applying a VSS source, i.e. you are using the device in single supply mode, then you need to put link K4 to position "B". Please see the user guide available on the evaluation board page:

    http://www.analog.com/en…

  • RE: multi-channel voltmeter

    Hi Giles,

    The ADG2128 is a 8 x 12 crosspoint switch which means that any of those 8 channels can be connected to any of the other 12 channels and vice versa. So that means there are 96 possible switch channels.The part is also fully specified for 12V…

  • AD75019 on resistance (2)

    Hello,

    I have asked about AD75019 on resistance.

    AD75019 on resistance 

    The customer wants to know the trend of characteristics of AD75019 on resistance .

    He read AN-251 and he ask me the configuration of AD75019 switch.

      1. Is AD75019 switch consist…

  • EVAL-ADG2128EBZ: What type of cable can I use to connect the board to my signal generator?

    I want to evaluate the chip ADG2128 for my application, what type of cable can
    I use to connect the board to my signal generator?

     

     

    The connector used on the EVAL-ADG2128EBZ is an RCA Jack, dual type, right
    angle/PCB mount.
  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225