Hi MDenomme955,
The ADG1636 has a Break-Before-Make Switching action so there should not have shoot through at the output of the switch.
Let me know if this helps.
Regards,
May
Hello;
In ADG1636 datasheet; why the power consumption would increase so much when Digital inputs=5V?
And in this case; what pin does Digital inputs mean? IN+; EN?
Many thanks;
Bell
I am looking for analog switches. The first is SPDT two channel. It must be capable of switching between a 0 to 14v square wave signal and a -5 to +14v zero crossing square wave signal. Current less then 10mA The second is SPDT two channel. It must…
I want data about ADG1636.Isn't there following data?
"Large Signal Voltage Tracking vs. Frequency" like ADG5436F.
"IDD vs. Logic Level" like ADG1219.
I would appreciate if you could give me some data.
Best regards,
Hello,
I would like to inquire about the power-off protection function of the analog switch being designed.
The problem product was ADG1636, and a warning light(12V power supplied) was turned on while the switch supply voltage 12V was not supplied. …
Hi Vincent,
The ADG836L, Dual SPDT/2:1 MUX and is capable in operating at Single Supply from 1.65V to 3.6V only. It is specified to accept Analog Signal Range of 0V to Vdd only. It will not accept negative input voltage.
ADG1636 on the other hand is…
Allow me to clarify. The original image I posted with the two comparators and the AND gate was to illustrate a window comparator. It provides three logic outputs that represent the three states you are looking to detect. That circuit does not output the…
Hi Emilzacharia,
From my understanding of the schematic above:
设计资源推荐
Circuits from the Lab