Good morning,
I am planning to control the switch AGG1611 with a digital output 5 V from Arduino. I saw that the input is 3V-compatible. Is it possible to use directly the Arduino 5V output or I need to reduce it?
Thank you,
Alessandro
Good morning,
I am planning to control the switch AGG1611 with a digital output 5 V from Arduino. I saw that the input is 3V-compatible. Is it possible to use directly the Arduino 5V output or I need to reduce it?
Thank you,
Alessandro
我是要用在一个给电容充放电的电路中,而且是一个从输入到输出,从输出到输入都由一个控制逻辑控制,通俗点说就是单刀单至。我目前选了一个ADG1611,不知道合不合适。ADG1611是四通道的,我想用双通道的。您有合适的给我推荐一些,谢谢。
谢谢,我的电路是AD620+AD8037,使用ADG1611调节AD620的增益,使用ADG1611的时候存在这个270KHz的噪声,我又重新制了一块电路板,没有使用ADG1611,就没有噪声了,应该是ADG1611的原因
Brian
Thanks for your response. I meant to say ADUM4121 instead of ADUM1421.
The opto-isolators in the drive provide isolation between the drive's internal high voltage electronics and the low voltage (5V) digital interface to my micro-controller. My…
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |
Hi,
From a performance viewpoint, the ADG1611 has lower leakage than the ADG4612.
However, the ADG4612 offers additional benefits in terms of being guaranteed Off without power so it really comes down to how the part will be used in system.
If you…
Hi dananderson75,
As you are using the audio band I would expect that flicker noise is present in the lower portion of the band. However as THD+N is very low in this region I would expect that the noise is low. As the SSM2402 is on a different process…