Is there an LTspice model for the ADG1609? If not, are there plans to provide one?
John
Is there an LTspice model for the ADG1609? If not, are there plans to provide one?
John
Hi all,
I would like to use the multiplexer ADG1609 for gain control in a fully differential ADC input stage and I need the spice model for it.
I post the same request on March 2014 and the Analog Support replied the model would be available after a…
Hi,
I am using ADG1609 MUX and AD623 and AD7685 ADC
My source is low input impedance(100 ohm) differential accelerometer.
I have few doubts about the Multiplexer and its inputs:
1.I think ADG1609 does not have internal protection diodes hence I am…
Hi,
In CN0354 the ADG1609 is operating using a +/-5V supply. The ADG726 cannot operate with these supplies, the maximum dual supply is can operate with +/- 2.5V.
Maybe using multiple ADG1609 is an option?
Regards,
Stephen
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |
Hi Andre,
The ADG759 cannot be used as the voltages used may damage the part.
As an alternative would the ADG1409 (which is specified at +/-5.5V) or the ADG1609 (which is specified at +/-5.5V and 3.3V, but can be operated at +/-3.3V) be of use? The…
Hi Theresa,
I have changed both mux ADG1409 by two mux ADG1609. I have the same problem. Must I insert a resistance between DA pins? I don't understand the problem...
I have a doubt with ABSOLUTE MAX RATINGS and CONTINOUS CURRENT PER CHANNEL, S…
Hi Tim,
We haven't characterized the device with VDD=5V and VSS=-0.5V as you suggest in your circuit, so we cannot guarantee its performance and reliability. However, the device will be functional and I expect similar performance to the single 5V supply…