• ADG1606 (TSSOP)

    Greetings All, 

    I am having trouble driving the Enable input of the ADG1606, with the GPIO output of a TI MSP432E4. The 1606 is connected to a unipolar source (12V, and GND) as shown in the schematic. When attempting to drive the input high, the Maximum…

  • AD7766, ADG1606

    Dear sir

    I want to use AD7766 to convert 16ch. (maybe 32) analogue input to digital.

    First question:

    To do that, I need an analogue MUX, concerning to noise and leakage current,  ADG1606 is a good choice or no ? if no, can you propose an analogue…

  • ADG1606: Unused pins S11,12,14,14,15,16

    Hi,

    I was wondering how to handle the input/output pins S11-16 if I don't plan to use them. I only need 10 input pins now, might expand later to use the other 6. But for now how should the unused pins be handled? Also, can pin 28 be left unconnected…

  • ADG1606 ESD protection

    Hi,

    I use an ADG1606 and others analog muxes in an analog front-end stage.

    The ADG1606 serves to multiplex the excitation current required to acquire 16 RTD sensors.

    I cannot use resistors in series with the inputs of the multiplexer.

    It's preferrable…

  • ADG1606 & ADG1604 Spice models

    Hello engineer zone team,

    i want to use the ADG1606 and the ADG1604 multiplexers in my circuit.

    First at all i want to simulate the circuit with a spice software.

    I cant find any spice model on your site.

    Do the spice models exists for this multiplexers…

  • Problem with ADG1606 protection

    Hello,

    We use an ADG1606 MUX as the final stage of our circuit to connect to external units (Hot unplug condition is normal in our application). From datasheet, I understood that "Overvoltages at IN, S, or D are clamped by internal diodes. Current should…

  • Migrating from ADG1606 to ADG726

    Dear EngineerZone Experts-

    Thanks in advance for your help. My team is currently using two analog multiplexer ADG1606 chips to control 31 signal channels. The PCB power is +/-5v. Due to some new design specifications, we will now power the PCB with a…

  • ADG1606 max current consumption at 150C?

    I would like to confirm what would be the max Current consumption for ADG1606 (power supply +-8V) greather than 125C i.e.150C?

  • 10mVp-p, 1nAp-p Signals Through ADG1606

    I am designing a calibration board that switches in different precision resistors to calibrate a resistance meter in an automated way. I was looking at using the ADG1606 to switch among several different resistances, and a 10mVp-p 100kHz signal will be…

  • Can ADG1606 conduct current from 'S' to 'D'?

    Hai, 

    In my design I need to multiplex 16 analog signals (current sources - 50mA max). This multiplexed current source will be connected to one resistor load of around 22 Ohm. Voltage across this load will then be given to ADC for data acquisition.