• ADG1604 - Waveform change when connect input to source terminal

    Hello,

    I'm using ADG1604 for channel selections. The input singal is sinwave, 50 Hz.

    When I connect the input to the ADG1604 terminal, the signal waveform is changed alot.

    1. My Schematic

    2. The orginal input waveform

    3. Input signal waveform when…

  • 模拟开关ADG1604

    你好,请问能不能单极性电源供电处理有负值的双极性信号?

  • ADG1604 DC "Off resistance"

    Can you perhaps give me an indication of the DC off resistance between each
    input and the output of ADG1604?

     

    We don’t measure DC OFF Resistance but we do measure the OFF leakage with
    voltage stress across the switch.  The Off R can be…
  • ADG1604有过压保护电路吗

    ADG1604有过压保护电路吗

  • RE: Dealing with ADG1604 Crosstalk

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADG1606 & ADG1604 Spice models

    Hello engineer zone team,

    i want to use the ADG1606 and the ADG1604 multiplexers in my circuit.

    First at all i want to simulate the circuit with a spice software.

    I cant find any spice model on your site.

    Do the spice models exists for this multiplexers…

  • I am using ADG1604. What are pins needed Pull up and pull down resistors ? Please suggest the resistor values.

    I am not getting proper results with ADG1604. please help me on pull up and pull down resistor values.

  • RE: ADG804 : maximum peak current

    Hi Ysuzuki,

    Can you share more information of the customer's application? I'm curious of the 3.5ms single pulse application.

    The Absolute Maximum Ratings ADG804 Data Sheet shows that Peak Current, S or D = 500mA is valid if the current is pulsed…

  • RE: ADG704 not work for photo diode switching

    Regarding the photo-diodes is a current source and than at the multiplexer the current flows from drain (D) to sources (S1, S2, S3 or S4), you need to have differential power supply at the multiplexer ADG704. ADG704 is only single supply operation, so…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225