• ADG1438 and ADG1439 switches input voltages in single-supply mode

    Based on the information from the data sheet I assume these switches can be powered in single-supply mode with Vdd up to +25V max. (Vss and GND connected together) with safe input voltages within 0V to Vdd range with any internal switches configuration…

  • ADG1439 current consumption

    Hello,

    I need to serially control 8 switches, every 7ms I need to open one channel for each switch and closed it 100 us after.

    For a clock of 30MHz which is the expected power consumption? How to minimize it?

    Thanks

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • RE: ADG1409 for switching power supply

    Hi Joaquim,

    The new SPI sequence is fine, no delays required.  Issue was that EN and Ax were being activated at same time, whereas its expected that the part would be ENabled prior to Ax control logic being driven.

    Btw, we have diff 4:1 mux with SPI…