Hi,
i'm testing an ADG1438 but i have a crasstalking issue.
In the allegated image the red wave is the correcect switch output that working correct, the yello is an other switch that is supposed to be off but i have a small signal. The issue is…
Serial Write Operation is attached. For Serial read Operation, no Timing Diagram
Hello,
Do you have an evaluation board for the ADG1438 8:1 mux chip?
Sincerely,
Vinson Go
Triangle BIoSystems
Based on the information from the data sheet I assume these switches can be powered in single-supply mode with Vdd up to +25V max. (Vss and GND connected together) with safe input voltages within 0V to Vdd range with any internal switches configuration…
Hi David,
We dont have +/-10V Differential 16:1 or 32:1 mux.
The highest channel count +/-10V or +/-15V mux we have is Diff 8:1 or 16:1 mux. These have parallel interface.
Low Ron option is the ADG1406/7 http://www.analog.com/en/switchesmultiplexers…