• ADG1436

    To use ADG1436 for +15V/-15V analog signal, I want to connect VDD to +15V, VSS to -15V. And I want to connect the ENABLE pin of LFCSP ADG1436 to +15V. And use 5V/0V as control signal for IN1/IN2. Is it OK?

    Thanks!

  • adg1436

    Hi,

    I'm having trouble understanding the logic table for the ADG1436, since table 7 doesn't seem to match the block diagram.

    Does ON mean connected?

    If using the TSSOP package, what is the default state if INx is floating (during power-up)…

  • ADG1436 with Asymmetric Supplies

    Is it okay to run the ADG1436 with VDD = +12V and VSS = -5V? I have an analog signal that is nominally 0-10V that I would like to switch but it may dip below 0V due to noise and I'd like to capture that information. Thanks.

  • ADG1436 leakage current

    Hi,

    We are trying to interface ADG1436 as a built in test component for a k type amplifier circuit. For normal operation, there seems to be leakage current that flows at any point of time. No complete isolation. This affects the amplifier's gain and…

  • ADG1436 with Single 28V supply

    Hello,

    I am interested in finding out if i can use the ADG1436 with a single supply of 28V (Vss = 0) ? It is below the absolute max rating of 35V, but the datasheet does not show results above 12V single supply, so i wanted to verify if we get good performance…

  • ADG1436 with Single 28V supply

    Re-posting this question, as there was no response...

     

    I am interested in finding out if i can use the ADG1436 with a single supply of 28V (Vss = 0) ? It is below the absolute max rating of 35V, but the datasheet does not show results above 12V…

  • ADG1436 Leakage current and latch up

    Hi,

    I am planing to use ADG1436 with Enable option in ultra low power application to switch load ON and OFF. VDD=+16V and VSS=GND. Inputs are connected to VDD/VSS and controls (INx and EN) are 3V compatible. 

    In shutdown mode VDD won't be present (since…

  • Problem with ADA4004-4/ADG1436/AD7628

    Dear All:

    Recently I had a full board using, among others, the chips named above. As I got ADA4004 or ADG1436 burnt without any explanation, I did a prototype board using only the above chips to try to discover the problem and still have the same problem…

  • ADG1436 是汽车等级吗?

    ADG1436 是汽车等级吗?

  • ADG1436 or general error analysis of analog switch.

    Hello,

    I have precision amplifier with three fixed gain step, 3x AD8021 with gain 10x, 50ohm sysem, frequency order MHz (DC decoupled),

    Gain is selectable over three ralays.

    In next generation I thing about replacing relay any analog switch , for…