ADG1413与ADG613封装和定义一致,唯一的区别在于供电。我的电路设计上使用ADG613时,±5V供电正常使用。当换到ADG1413时,仅±5V供电时能正常工作,+12V供电和±15V供电下均会烧毁。这与其datasheet描述不太相符。请问会是什么问题么?
ADG1413与ADG613封装和定义一致,唯一的区别在于供电。我的电路设计上使用ADG613时,±5V供电正常使用。当换到ADG1413时,仅±5V供电时能正常工作,+12V供电和±15V供电下均会烧毁。这与其datasheet描述不太相符。请问会是什么问题么?
Hello ,
You mentionned that the ADG1413 exists on AEC Q100 qualified version , but no MPN available to buy ithe W sufix .
Can you please support us to find the searched part ?
Regards
Hi Kyle,
Thanks for highlighting this. I will get this updated. In the mean time, you can use the data for either the ADG1411 or ADG1413, the data for the ADG1411, ADG1412 & ADG1413 is all the same.
Regards,
David
Hi,
he customer is considering using ADG 1413 and received questions about the simulation.
In the circuit diagram below, when using the ADG 1413, when inputting a 10 V signal, the output was only about 4 V.
Even if it is changed to other conditions, only…
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |