• RE: Paralleling analog switches to lower on-resistance

    I would like to refine the second part of my inquiry.  I am using an ADG1409 to route one signal (connected to common “D”) to different destinations.  I only need two destinations at the present.  The other two “S” outputs – can they be left unconnected…

  • RE: higher dual voltage on ADG759

    Hi Andre,

    The ADG759 cannot be used as the voltages used may damage the part.

    As an alternative would the ADG1409 (which is specified at +/-5.5V) or the ADG1609 (which is specified at +/-5.5V and 3.3V, but can be operated at +/-3.3V) be of use? The…

  • RE: getting analog switch common mode down to -0.10V

    Hi Tim,

    We haven't characterized the device with VDD=5V and VSS=-0.5V as you suggest in your circuit, so we cannot guarantee its performance and reliability. However, the device will be functional and I expect similar performance to the single 5V supply…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • ADC architecture choice

    Hello,

    I schould design a load cell signal chain. My configuration is:

    - load cell: 0.55mV/V at 5000kg

    - load cell supply: not define yet: 5V give a poor sensibility. I think 8V is good because my system schould work between 9V - 16V.

    I can not go…