• Surge damage in ADG1402

    Hi,

         In my project to measure analog voltage or current,  I'm using ADG1402 analog switch to connect or not a shunt resistor used to measure input current in a system with a ADC. My input is differential and protect against differential surge using a…

  • Guard on ADG1402 analogue switch

    Anonymous
    Anonymous

    Is pin 2 on your ADG1402 analogue switch internally connected or can it be used to guide a guard ring around pin1?

  • RE: ADG1402BCPZ

    Hi Kazu,

    Unfortunately, the ADG1402 is not operational at +/-3.3V supply rails. This is stated at the Power Requirements table at the Specifications Section of the datasheet. Please see screenshot below.

    For Dual Supply Operation, the minimum voltage…

  • Single SPST analog switch with power off protection

    Hello,

    I search an analog switch with the following characteristic :

    - single SPST - NO (like ADG1402)

    - dual supply +/-5V - +/-15V or single supply +5V - +15V

    - analog input +/-3V

    - power off protection (like ADG4612)

    - SMT Package

    Is the a component…

  • AD8429 gain switching

    For a data acquisition frontend we need an instrumentation amplifier with wide bandwidth, low distortion, and low noise. We are considering the AD8429. The frontend needs to capture signals with +/-10V, 1V, and 100mV full-scale range, requiring to switch…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225