• ADG1401 Datasheet

    Hello,

    I was looking for ADG1401 datasheet. I saw that with +/- 5 V dual supply the Analog Signal Range goes from 0 to VDD [V] (Page 5 of datasheet). My question is if it is correct? I'm asking that because all other switches of the family goes from…

  • ADG1401 simulation (SPICE)

    Hello,

    I see that there is no spice model available for the ADG1401 part.

    Do you have any recommendation on how can I simulate it (even being not accurate)? I thought of adapting some similar part, and just change specifications in the spice model.…

  • RE: ADG2188

    3) Propagation Delay time

    I have the same question with ADG1401. I want to use AD1401 as feedback path in AD8057.

  • RE: Analog switch for low noise DC

    Hi,

    The ADG1419 would also be my recommendation.  Switches with lowest Ron and Ron flatness are best for switching precision DC signals.  This has 2ohms Ron and very good Ron flatness.  Minimum Ron flatness ensure minimum signal distortion through the switch…

  • Analog switch for 100Mhz

    Dear Sir,

    I am looking for an analog switch with the following features:

    • Working frequency: 1Mhz to 100Mhz
    • Rdson < 2 ohms
    • low Rdson flatness
    • insertion loss = 0.5dB aprox (from 1Mhz to 100Mhz)
    • Vdd: 10Vdc

    I want to use an analog switch…

  • RE: Guard on ADG1402 analogue switch

    I like it very much with the ADG1401/1402 that the one NC pin is pin 2 so it can be used for routing a guard ring around pin 1.

    I would have loved it, though, if the second NC pin would have been pin 7 instead of pin 5, so it would have been possible…

  • RE: adding variable gain to AD8222

    Thank you for the response. I was looking to set the gain to 1 or 25. and since I have 16 of them on a card I was looking to use the AD1414 directly to switch in the gain vs using like an ADG1401 that can be put really close to the part. Again the gain…

  • RE: Audio switch

    HI Teodor,

    Thanks for the clarification,

    For the single SPST request have a look at the ADG1401. Very low Ron & Ron flatness and this is available in a 8-Lead MSOP or 8 LEAD LFCSP package.

    Details here: http://www.analog.com/media/en/technical…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225