Hi I am using the ADG1211 is my application board simulation ( downloaded the spice model for AD website). When the switch is off that time I am seeing 500nA of leakage but the data sheet says that it is few pA. Can anybody help me about this.
Hi I am using the ADG1211 is my application board simulation ( downloaded the spice model for AD website). When the switch is off that time I am seeing 500nA of leakage but the data sheet says that it is few pA. Can anybody help me about this.
Hi All,
Can I use 15V/0V for INx pins (Logic Control Input pins) under VDD=15V and VSS=-15V conditions?
Also, ADG411 and ADG1411 can be used same conditions?
Best Regards,
Kazu
Hello,
Our design uses electronic keys for switching very weak and relatively low frequency currents. And it is very important that its capacitance Coff (source/drain; RFx/ RFC) would be 0,1...0,2 pF, range begin with 0 Hz (DC)… to a few kHz, and it would…
Hi Ntroise,
Sorry for the late response.
The track-hold setup time is the time interval before the input voltage is sampled for each tracking cycle in the PWM signals driving the ADG1211 switches. The track-hold hold time the time interval after sampling…
The power solution in this interactive document offers a detailed summary of the power supply design for each scenario in the Lowest Noise and Drift signal chain option.
The document includes the power requirements, the block diagram and power tree, and…
And the ADG1211 has the definition of LOWONSWITCH, while I still didn't find the prototype of HIGHONSWITCH subcircuit.
Hi jebaspaul,
Unfortunately ADI does not currently have a SPICE model for the ADG1207. We do provide a model for the ADG1211. This model can be configured to be representative of the ADG1207. The model can be found at the link below.
Hello.
I'm working on a project that includes dozens of the following devices: AD5260, AD5290, ADG1211, ADG1212, ADG1414.
I understand from their respective datasheets that voltage rails should be powered in a specific order: GND, Vdd/Vss, digital…
Hi,
Unfortunately we do not have a spice model available for the ADG1611 at this time.
What supplies are you using for the ADG1611 model?If the ADG1211 model is simulated with a dual 5V supply the model will not function properly. The ADG1211 is optimized…
您好!
我想设计一个用于水质电导率测量的小型设备,因为看到你们的CN0359全自动高性能电导率测量系统的宣传性能不错,我购买了评估版并做了几块测试板进行测试验证,发现至少有3块板子(包括购买的原装评估板)发生莫名其妙的故障。最近有空进行了逐一排查,发现几个问题如下:
1、故障电路板-1:原装评估板。上电过程中,D2(1N4148W)出现冒烟,±15V无法输出(L5的3.3V输出正常)。经过排查,发现U15(AD8253ARMZ)的VDD与VSS已经导通!这导致整个电路板的+15V与-15V网络导通…