• RE: ADF7241 SPI RC_READY bit getting stuck at 0

    Hi Aldrich,

    Unfortunately the issue was never resolved, however, I have been able to work around it by resetting the radio whenever the RC_READY bit gets stuck. With this fix the resets occur every 10-15 minutes or so, but allow normal operation to resume…

  • ADF7242 / ADF7241 with an External PA and LNA

    Where can I find an example of the ADF724x with an external PA/LNA?

  • ADI年度贺岁片——构建Zigbee的无线射频技术芯片ADF7241系列

    ADI年度贺岁片——构建Zigbee的无线射频技术芯片ADF7241系列 by yaof

        ADF7241适合电池供电系统,具有一个灵活的双端口RF接口支持交换天线多样性 。ADF7241支持IEEE 802.15.4兼容的DSSS - OQPSK调制为250 kbps的比特率从62.5 kbps的2 Mbps的比特率,同时还支持FSK和GFSK调制。 ADF7242还有一个内置电池监控功能,具有非常低的功耗,使用ADF7241完全集成的低成本,短距离,低功耗的收发器设计用于在全球2…

  • Reduce ADF7242 / ADF7241 BOM count with a discrete RF Balun

    Where can I find an example of the ADF7241 or ADF7242 being used with a discrete Balun?

  • Using the ADF7242 or ADF7241 to implement Automatic IEEE 802.15.4-2016 Operating Modes

    How can I implement automatic IEEE 802.15.4-2016 Operating Modes using the ADF7241 or ADF7241
  • ADF7241状态问题

    求助:我按照ADI的评估板制了一块ADF7241的PCB。焊好之后发现用SPI写SPI_NOP命令的时候读出来的状态字是0x81,要么是0x82,或者0x83。就是说一直没有RC_READY这个标志位置位。也就是说无线电管理器一直没有准备好。请问这是为什么。

  • ADF7241的PHY_RDY状态

    各位好,我现在在使用ADF7241DB1Z,没有使用配套的mother board,只连接了SPI的接口和电源线,每次上电之后只能在IDLE,SLEEP和MEAS状态间转换,在IDLE状态进入PHY_RDY时,返回的状态值为0xFF,之后就无法做任何操作了,除了重新进入IDLE状态。

    这是为什么呢?求个位指导!是否在进入PHY_RDY前需要做什么设置?

  • ADF7241的状态转换

    您好,我用pic24的单片机控制该收发器,选用SPI通信。上电之后,查看状态为0xE1(IDEL状态),然后移入CMD_RC_RESET,查看状态为0xE0(不知是否为SLEEP状态),之后拉低拉高CS,查看状态为0xE1(IDEL状态),最后想移入CMD_RC_PHY_RDY进入PHY_RDY状态,可是MISO的返回值一直是0xFF,不明白这是什么意思?请大神指导。

  • ADI年度贺岁片——构建Zigbee的无线射频技术芯片ADF7241系列

        ADF7241适合电池供电系统,具有一个灵活的双端口RF接口支持交换天线多样性 。ADF7241支持IEEE 802.15.4兼容的DSSS - OQPSK调制为250 kbps的比特率从62.5 kbps的2 Mbps的比特率,同时还支持FSK和GFSK调制。 ADF7242还有一个内置电池监控功能,具有非常低的功耗,使用ADF7241完全集成的低成本,短距离,低功耗的收发器设计用于在全球2.4 GHz ISM频段的操作。

       采用该频段进行ZIGBEE协议有关物联网技术的设计,是未来互联网技术升级的方向…

  • RE: ADF 7241/7242 Receiver

    Hi,

    The external components on the evaluation board is recommended. You may find the circuit in the ADF7241/ADF7242 Evaluation Board start guide which is installed with the evaluation software.

    Regards,

    Aldrich