• ADF7024 and AN1309

    Hi,

    I found AN1309 which is application note for using ADF7023 + RFFM6901(PA).

    Can I apply this for ADF7024? If so, Is there anyone can provide related information?

  • ADF7024 Design Resource Package

    Register and download the ADF7024 design resource package by following this link

    The ADF7024 design resource package includes the following:

    • ADF7024 reference manual
    • Schematics, Gerbers and BOMs for the ADF7024 evaluation boards
    • Application…
  • Data rate by ADF7024 profiles

    My customer compared the transmission time of ADF7024 between Profile D and E. In theory, they expected to reduce the transmission time by half, but they could not find a difference between the two profiles.

    Please help the customer improve the problem…

  • Radio profiles with ADF7024

    Original Question: Radio profiles with ADF7024 by NagarjunaG

    I see only 6 radio profiles recommended in this offering with ADF7024. Can I create my own radio profiles to suit my requirements beyond these suggested profiles?


    Verified Answer: RE: Radio…

  • TX/RX time when using ADF7024

    Hi,

    My customer wants to transmit and receive 131bytes data using ADF7024.

    How long does the overall transmission time when using the radio profile D?

    If they use the radio profile E, How much can they reduce the overall transmission time than using…

  • Impossible to download ADF7024 design resource package

    Hi,

     

    When I try to download ADF7024 Design Packages for Low Power RF Transceivers | Analog Devices I get nothing. How could I find ADF7024 Reference Manual, UG-698? Thank you in advance.

     

    Regards,

    Ivan

  • FAQ: ADRadioNet radio profiles with ADF7024

    I see only 6 radio profiles recommended in this offering with ADF7024. Can I create my own radio profiles to suit my requirements beyond these suggested profiles?

    ADRadioNet is not restricted to operate in any particular radio profile, however the…

  • Range of ADF7024 inside a multi storey building

    How far I can receive data from one floor of the building to another floor of the same building? I am not getting more than one floor away from the transmitter. Both transmitter and receiver are ADF7024 ICs.

  • Running the ADF7024 from the ADuCM3029 board using IAR?

    I would like to run the ADF7024 from the ADuCM3029 eval board. I have IAR installed, should I use that, is there example code available?