• ADF7023-J RF transceiver sport mode

    Hi all,

    what is sport mode control in ADF7023-J chipset?

    I want to interface ADF7023-J with Cypress PSOC5 controller.

    My project demands a Half Duplex RF modem with Frequency Hopping.

    Is ADF7023-J able to do it at 57.6Kbps datarate?

    Regards,

    ra…

  • ADF7023-J TEST PROGRAM

    Hi

    My customer started the experiment focusing on ADF7023-J.
    For now they are checking the specifications of the data sheet in order.
    ADI 's site introduces a wonderful module to extend the capabilities of the device.
    Is there a rudimentary sample program…

  • ADF7023-J VDDBAT1/VDDBAT2

    Hi,

    About power supply VDDBAT1/VDDBAT2 of ADF7023-J,
    is it possible to supply power to VDDBAT1/VDDBAT2 from different sources.
    For example,
    VDDBAT1 is supplied from a 2.2V source.
    VDDBAT2 is supplied from a 3.3V source.

    We would assume that VDDBAT1/VDDBAT2…

  • ADF7023-J的简单单片机控制经验

    *小白一只,求问ADF7023-J这款芯片可不可以由简单的单片机进行控制?求助攻

  • ADF7023-J

    Hello,

    I would like to know if it’s possible to use two ADF7023-J on two different PCB to track each other. I would have a "TX" board and a "RX" board. I want to trace the "TX" board without moving the "RX" board around (if possible…

  • ADF7023-J initial code

    Hi,

    Could ADI provie the initial code of ADF7023-J?

    We want to use ADF7023-J and we will be appropriate if there is some initial code. We don't want to begin from nothing.

     

  • Crystal Oscillator for ADF7023-J

    Hello,

    I have a question about ADF7023-J.

    Are there any specifications regarding the voltage level required for the crystal oscillator used in the ADF7023-J?

    Best regards,

  • Software drivers for ADF7023-J

    I have a design using the ADF7023-J xceiver and was trying to pull in software to initialize & configure it with my Atmel micro. I downloaded the adf7023.c and adf7023.h files which appear to have the required functions but they reference include.h which…

  • J-B and J-C Thermal resistance for LTC2991IMS

    hI.,

    I need J-B and J-C Thermal resistance for LTC2991IMS. I get only J-A thermal resistance in datasheet.

  • ADF7023 EVB PCB files

    Hi Sir,

    We are going to design a sub-g transceiver by ADF7023 , We would like have a reference with EVB and file the geber file from below , but could you help to provide PCB layout (ex: allergo or power pcb) to us?

    http://www.analog.com/media/en/technical…