Hi!
I am working with the ISM transceiver ADF7021-N and I´d need to know the value of the frequency , by default, of the CLKOUT signal from the SPI interface.
I can not find it on the datasheet,
Thank you very much,
María.
The ADF7021-N allows a C4FM TX mode using a Root Raised filter, but the corresponding mode for RX has a placeholder (Reserved) in the Register 4 SETUP (DEMOD_SCHEME).
Surely this has been implemented and is only missing documentation?
Two EVAL ADF70xxMBZ2 boards with ADF7021-N daughter boards, set up per the Quick Start Guide instructions, one as Base Station the other as End Point In trying to perform a transmit test using the suggested serial# transmit demo we are getting an error…
Hello,
Beyond the Register 1 changes required based on the output frequency, are there any other register differences between the ADF7021 and ADF7021-N? I am trying to use the same register settings to support both the ADF7021 and ADF7021-N parts. Is…
In the eval board software for the ADF7021-N, the calculation for AFC seems to not allow the user to specify a XTAL frequency other than the default value (In my case, 12MHz). THis give an error in the calculated AFC.
It seems to work ok for the Non…
Hi All,
One of my customer is investigating a 351MHz and 467MHz digital wireless radio with 4-FSK modulation.
For this purpose, he is interesting ADF7021-N and ADF7021-V transceiver.
The frequency range and modulation mode of these transceiver are…
I am facing a strange issue with AGC on the ADF7021-N chip.
I am using an external oscillator at 14,7456 MHz, listening to a transmitter sending analog audio at 324,0875 MHz and my register settings looks like this:
reg0: 0x095f8c80
reg1: …
which is the best protocol to interface adf7021-N with a microcontroller and why
hi;
can u suggest me from where i can get adf7021-N hil software codes for the working of adftransceiver
is there a buffer inside a adf7021-N for sending data it received from transmitter to a micro controller if then what is its size