• ADF7020-1 is the serial port protocol similar to a standard UART?

    ADF7020-1 - I see that the electrical parameters are TTL or CMOS device compatible, just wondering if the protocol is similar to a standard UART? 

  • Issue with ADF7020-1

    We are able to configure the module as transmitter and receiver. The problem we are facing is that SYNC word detection by the ADF7020-1 module according to the data sheet is not happening.

    Our configuration ADF7020-1[TX] --------> ADF7020-1 [RX].

  • RE: I need help! ADF7020-1 is not in the ADI SRD Design Studio.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADF7020-1

    1, the linear correlation demodulation and demodulation eliminates the need for a preamble length differences, have any impact on the rest of the parameters?
    2, encountered in the use of the following circumstances:
    TCXO - 19.2MHz, PFD = 9.6MHz
    Modulation…

  • RE: ADF7020-1 参数配置问题

    感谢您的咨询。有关ADF7020-1类型的问题请您直接发送到ADI英文技术论坛咨询,谢谢!

    https://ez.analog.com/welcome

  • ADF7020-1 just want to confirm that the Tx/Rx Control port is for transferring the RF data in/out of the device, and the SPI is for control commands to the device?

    ADF7020-1 just want to confirm that the Tx/Rx Control port is for transferring the RF data in/out of the device, and the SPI is for control commands to the device?

  • ADF7020-1的接收问题

    请问我现在需要做一个ADF7020-1的接收机,采用FSK调制,频率在258M,9.38kbps不使用同步字,那么我读取FSK的数据的时候怎么看DATA_IO已经接收到了FSK数据呢,现在不知道为什么没有接FSK信号,DATA_IO也有高低电平,DATA_CLK也是9.38k,请问是什么问题呢?

  • how to interface adf7020-1 with stm32f4 ?

    can any one help me interfacing adf7020-1 with stm32f4 , nd how to set it as transmitter and receiver ?

  • RE: Questions for LTC6811-1, LTC6812-1

    Dear Abhishek,

    Thank you for your kind answer.

    But additionaly my customer asks that they want to know the maximum power specification of Zennor diodes in LTC6812-1 and LTC6811-1.

    (Its zennor diodes are located inside of LTC6812-1 and LTC6811-1 and Cx…

  • LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF

    Could anyone explain what 3NS means on part numbers such as LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF ?

    I cannot find any information.

    thank you