• RE: ADF7020-1 Register settings for FSK modulation

    Hi V Rajendra,

    Correct register settings are found in the ADF7020-1 Data Sheet. I would suggest using configurations in the Datasheet using an ADF7021 eval board and the ADF7021 eval software as these configurations were tested working, then try your configurations…

  • TCXO with ADF7020-1

    Hi.
    I have noticed that the ADF7021 transceiver has an option for a 0.8Vpp TCXO reference via pin OSC1, and the ADF7020-1 does not state that option in its datasheet. Is that the case, or is it possible in the same manner?

    Thank you, Kosta

  • ADF7020-1 manual register edit

    I use ADF7020-1 EVAL and want edit register.

    I tried to change the register in the manual register edit. but didn't change.

    How can i edit the register? 

    please some  advice.

  • EVAL-ADF7020-1DBZ6 in Burst Mode

    Hello,

    is it possible with the EVAL-ADF7020-1DBZ6 to operate in burst mode, which means, that I would like to transfer data in time multiplex with another device?

    How can I configure the module for this?

    Thanks!

    Best regards

    Winfried

  • Issue about ADF7020-1

    HI.

    I'm jeongtae kim from south korea.

    I have a issue which use the ADF7020-X Config SW.

    I want to observe the RSSI value in EVAL-ADF7020-1DBZ5 board with EVAL-ADF70xxMBZ2 board.

     

    In order to use that i open the Manual Register Edit and write the register…

  • RE: Proper application of ADF7020-1?

    Hi,

    To answer your questions,

    1. The ADF7020-1 would suffice, however, Support for the ADF7020 and ADF7020-1 are no longer provided here in EZone. For better overall performance and support, I would like to suggest for you to look into the ADF7021 line of…

  • RE: In ADF7020-1, why interrupt is fired even Master is off?  Is ADF7020-1 check for valid sync byte for generation of interrupt?

    Hi Polmon,

    Regardless of the status of the master, as long as power is still applied to ADF7020-1, it will continue operating as it was previously configured.

    For ADF7020-1, interrupt can only be generated by sync word detection.

    If configured to do so, the…

  • ADF7020-1 SW Register setting Issue

    HI.

    I'm jeongtae kim from south korea.

    I have a issue which use the ADF7020-X Config SW.

    I want to observe the RSSI value in EVAL-ADF7020-1DBZ5 board with EVAL-ADF70xxMBZ2 board.

     

    In order to use that i open the Manual Register Edit and write the register…

  • RE: is re initialization of ADF7020-1 generates interrupt?

    Hi Polmon,

    Even if the master is off, the ADF7020-1 will continue operating as configured, as long as power is still applied to it. So, it will remain in the Rx state and will continuously receive data until instructed to go to another state.

    The INT…

  • RE: ADF7020-1 question

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,