• RE: ADF7020-1 Register settings for FSK modulation

    Hi V Rajendra,

    Correct register settings are found in the ADF7020-1 Data Sheet. I would suggest using configurations in the Datasheet using an ADF7021 eval board and the ADF7021 eval software as these configurations were tested working, then try your configurations…

  • TCXO with ADF7020-1

    Hi.
    I have noticed that the ADF7021 transceiver has an option for a 0.8Vpp TCXO reference via pin OSC1, and the ADF7020-1 does not state that option in its datasheet. Is that the case, or is it possible in the same manner?

    Thank you, Kosta

  • Issue about ADF7020-1

    HI.

    I'm jeongtae kim from south korea.

    I have a issue which use the ADF7020-X Config SW.

    I want to observe the RSSI value in EVAL-ADF7020-1DBZ5 board with EVAL-ADF70xxMBZ2 board.

     

    In order to use that i open the Manual Register Edit and write the register…

  • ADF7020-1 manual register edit

    I use ADF7020-1 EVAL and want edit register.

    I tried to change the register in the manual register edit. but didn't change.

    How can i edit the register? 

    please some  advice.

  • ADF7020 Software Reference Manual

    Hello,

            Does ADF7020 has software reference manual, just like UG-1002 for ADF7030-1. Or could you advice how to set the state of  interface such as RXCLK&RxDATA.

  • ADF7020-1 SW Register setting Issue

    HI.

    I'm jeongtae kim from south korea.

    I have a issue which use the ADF7020-X Config SW.

    I want to observe the RSSI value in EVAL-ADF7020-1DBZ5 board with EVAL-ADF70xxMBZ2 board.

     

    In order to use that i open the Manual Register Edit and write the register…

  • ADF7020 Eval Board Pinout

    Hello there,

    I've bought the EVAL-ADF7020DBZ3 daughter board not knowing that there's a dev kit board that can be bought separately. Unfortunately, I don't have the finances to purchase that board/kit.

    Is it possible to attempt interfacing with…

  • ADF7020 miss data,433MHz

    We used ADF7020 for TRx, and we used it to receive audio signal, it can work normal at 915MHz, but we missed some data at 433MHz, so we didn't know its reason why it can appear, do you have any ideas to explain it?

  • Proper application of ADF7020-1?

    Greetings community.

    I'm setting out to design a module for integration into a larger [wired] building management system that will listen on a fixed frequency (or better yet, cycle through a pre-defined batch of frequencies) in the NOAA weather radio…

  • RE: In ADF7020-1, why interrupt is fired even Master is off?  Is ADF7020-1 check for valid sync byte for generation of interrupt?

    Hi Polmon,

    Regardless of the status of the master, as long as power is still applied to ADF7020-1, it will continue operating as it was previously configured.

    For ADF7020-1, interrupt can only be generated by sync word detection.

    If configured to do so, the…