Hi,
As also discussed by mail, it is not possible to read Vtune voltage using the internal ADC. It is only for temperature readback purpose.
Regards, Kazim
Hi,
As also discussed by mail, it is not possible to read Vtune voltage using the internal ADC. It is only for temperature readback purpose.
Regards, Kazim
Hi Husnain,
ADF4371 outputs should be AC-coupled to SE 50Ω's or differential 100Ω.
It is not true to classify the output as square or sine wave. As you can see from Figure-15, the 3rd and 5th harmonics are significantly high which make…
Where can I find ADF4371 eval board ACE support? There is no selection from ACE pull down menu.
Hi,
Hi Matt,
Decreasing the CP current to min value changes the loop filter response. The default value is recommended for CP current. If you like to use a very narrow loop BW, it is better to design a new filter still using the default CP current (or slightly…
Hi ADI,
Is there any Python libraries available for the ADF4371?
Regards,
Chris
This is Motoki Moritani. I am a 1st year master's student, belongs to the Structural Dynamics Design Laboratory, Tokyo Institute of Technology.
I have a question regarding the radiation resistance of item ADF4371 that I found on your website (https…
I would like to obtain code samples (in any computer language) for:
- initialization of the ADF 4371
- setting the frequency output (fractional mode) with autocal enabled
- setting the frequency and any required calibration data with autocal disabled
…Hello,
I am experiencing a strange behavior when using ADF4371/4372 synthesizers - after some time of normal operation the IC starts to show a low impedance (around 1 ohm when measured with a ohm meter) at some ports - eg. the reference inputs or CP output…