• RE: ADF4360-7 Schematic

    All looks good.

    Also, see page 9 of the ADF4360-7 evaluation board user guide for reference: http://www.analog.com/static/imported-files/user_guides/UG-104.pdf#page=9

  • An issue about ADF4360-7

    Dear Sir/Madam,

    I  want to get a delayed 1.5GHz signal by  below solution. Delay the 10MHz input  signal of ADF4360-7 , and then get the delayed 1.5GHz signal at the output. however, I note that there is a delay unit in  ADF4360-7, and I wonder whether or…

  • ADF4360-7无输出!急求助!!

    外部信号源是10Mhz,产生433Mhz信号,电源管脚的电压全部为3.29v,滤波器是参照ADIpllsim做的,不过在做板的时候没有注意将L1和L2两个外部电感垂直放置,两个电感为22nh绕线电感。
    测试程序是参照ADF4360-8修改的,用c8051f020单片机控制,芯片内部无2分频,与分频采用8/9,无锁定输出。

    测试中R分频器有非常好的输出,200kHz梳状脉冲,这证明程序没有问题,且芯片工作了,晶振的信号也进来了。
    muxout接DVdd与DGND都有输出。
    但是muxout接N分频器是基本没有输出…

  • Band selection in ADF4360-7

    In my application, I need the band selected by the ADF4360-7 to be consistent.  Right now I see many boards where the loop is bi-stable - one with a control voltage of 1.2V and the other with a control voltage of 2.5V as I reprogram the device to the same…

  • ADF4360-7 as 500MHz clock source for AD9958

    Preamble: Maximum output power of AD4360 (-5dBm) is lower than recommended clock drive level for AD9958 (200..1000 mV). Moreover, I'm planning to split system by two or more boards - clock source on one board, DDS chip on another, controller on third…

  • ADF4360-7 HMCAD1511 时钟抖动

    现在用ADF4360-7的时钟输出HMCAD1511,要求均方根抖动为160 fs的时钟;ADF4360-7能满足要求吗?

    如果能ADF4360-7的参考晶振该如何选择?

    如果不能ADF4360-7能满足的最小时钟抖动为多少,参考晶振该如何选择?

  • the verilog code for ADF4360-7

         Hello,

         would anybody send me a verilog code for ADF4360-7.I‘m in trouble with it, and my code is not effective. I can't solve it!

         email:dingbin89@126.com

         Thanks.

  • ADF4360-7: Choosing the correct inductance value

    A question about ADF4360-7. If I need a RF out band 175-900 Mhz ( 350-1800 Mhz:2), how select external  inductors at pins 9-10  correct value ? I could  use the graphic figure 24 of  ADF4360-7 datasheet, but it's valid for 350-1800 Mhz RF band! Then...?…

  • ADF4360-7 generate 350 MHz by using 30 nH is ok ,but can not generate 1.0GH by using 3.1nH

    ADF4360-7 generate 350Mhz clock by using 30 nH to drive HMCAD1511 ,HMCAD1511 is work,

    oscilloscope can   see  the 350MHZ clock.

    but generate 1.0GH clock by using 3.1nH to drive HMCAD1511,HMCAD1511 is not work , 

    oscilloscope can not  see the 1.0GHZ clock.

    Is it…

  • ADF4360-7 Evaluation Board Design Files and Layout Description

    Hi, Could you please provide me EV-ADF4360-7EB1Z PCB design files, layouts thickness and materials used in each layout (FR4, Rogers, etc.)? Thank you in advance. Regards, Ivan