hello,i designed a pcb with adf4360-6,I have a problem with adf4360-6, i have try several days ,but it still unlock
The ref_clock is 9.8304MHz, and the RFout that I want is 9.8304*126 = 1238.6304MHz, the N out and Rout is right,the loop filter is
…hello,i designed a pcb with adf4360-6,I have a problem with adf4360-6, i have try several days ,but it still unlock
The ref_clock is 9.8304MHz, and the RFout that I want is 9.8304*126 = 1238.6304MHz, the N out and Rout is right,the loop filter is
…Hi,
The MUXOUT pin on the ADF4360 series has an option for SDOUT, please can you confirm what this does?
I can't seem to find any explanation in the datasheet?
It sounds like serial data out, does this mean its possible to read back register values…
Hi
first of all : excellent forum, nearly all of my questions solved by reading some posts. Good search function.
Now the situation and question:
1)
In our design we need a receiver LO frequency around 1100 MHz. Phase noise requirements are nearly…
The latest ADF4360-x software is attached. This is compatible with all the ADF4360 family.
Installation process:
1. Disconnect any evaluation board
2. Download and run the attached installer
3. Click Next/Continue/Finish when asked
4. Connect your…
Hi, I want to design Vin:20-31 V and Vout:270 V Pout=8 kW, 6-Phase Boost Converter. But I have lots of problem related design. Firsty, The design is not run available. INTVc pin is below 10 V. And 3,4,5 and 6th phase is not running correctly. Iam sharing…
Hi,
Is there any recommended footprint from Analog Devices which I could use to generate footprint (in PADS Layout) for ADP2127ACNZ1.260R7 (6-Pad Embedded Wafer Level Package [EWLP], CN-6-1 package)?
Regards,
Leong
The latest ADF4360-x software is attached.
Installation process:
1. Disconnect any evaluation board
2. Download and run the attached installer
3. Click Next/Continue/Finish when asked
4. Connect your evaluation board
5. Windows will detect the evaluation…
First of all thank you very much for your excellent forum, I'm doing a Design of an Economical Antenna-Gain and Radiation-Pattern Measurement System, for that I dispose of a adf4360 and AD8302 detector, my problem is with adf4360 when checking the…
How do we come to know that whether the synthesiser ADf4360-9 has been programmed properly or not...
I am a student I have a project am using ADF4360-0 module as frequency synthesizer, I have finished my PCB, now am in the programming stage ,I have some problem regarding programming, First of all I am using VCXO as reference frequency (20MHz) I want…