Hi, I am currently using the ADF4360-9 to generate an LO ref in the range 146-152 MHz. My phase noise requirements are quite strict so have ended up running the VCO at double this and using the Divout f/2 output to get a slight improvement in noise performance…
Hello,
I am using ADF4360-9 as a transmitter with FM modulator on the VCO (Vtune).
To ensure reliable performances on the modulation, I would like to avoid switching VCO band when varying across the temperature range.
I have already reduced the inductor…
Hello
I have started using EV-ADF4360-9EB1Z through GUI provided with the evaluation board. As default the "RF Output Frequency" is set as 360 MHz. As per datasheet, primary output range is 64 to 400MHz. When i enter 200 as "RF Output Frequency…
Dear team,
Could I know the difference between LT1964ES5-5#PBF and LT1964IS5-5#PBF?
It seems that these parts are same parts(performance, quantity)
The price difference is checked, but I don't know why.
hy,
in the data sheet of the ADF4360-0 frefin minimum is mentioned with 10MHz with an advice to couple below 10MHz via DC. I try to use 2MHz TTL-Signal to frefin with the result of large jitter on the R-Out monitored on MUXOut and no lock of the PLL.
…I bought the Ev-ADF4360-1EB1Z. When I look at the board, L1, L2, R25 and R26 are all not mounted.
Is this correct?
Dear
We are going to use LT8609AEDDM#TRPBF for our products to launch the market now, however we cannot get yor chips now seriously, so might be stopped ship our product.
Well maybe it is irregal idea but let me know, can we use the LT8609AHDDM-5#TRPB…