Hello Guys,
I want to know the diference between the LTC4267IGN, LTC4267IGN-3 and LTC4267CGN-3.
They are direct substitutes?
If not, what is the main difference between each one?
Thanks!!
Hello Guys,
I want to know the diference between the LTC4267IGN, LTC4267IGN-3 and LTC4267CGN-3.
They are direct substitutes?
If not, what is the main difference between each one?
Thanks!!
I have used ADI PLL Sim to generate a design for a 900 MHz CW local oscillator using an ADF4360-3. Currently I'm trying to work out how to program into the ADF4360-3 eval board based on the simulation file results. What should the RF output frequency…
hy,
in the data sheet of the ADF4360-0 frefin minimum is mentioned with 10MHz with an advice to couple below 10MHz via DC. I try to use 2MHz TTL-Signal to frefin with the result of large jitter on the R-Out monitored on MUXOut and no lock of the PLL.
…I bought the Ev-ADF4360-1EB1Z. When I look at the board, L1, L2, R25 and R26 are all not mounted.
Is this correct?
I have the evaluation board of ADF4360-3.
I want to access it using myRIO from National Instruments (NI). This device is Running Linux Real Time OS... If I have the .so library for this device i can access the device using Labview and MyRIO.
this is…
The power solution in this interactive document offers a detailed summary of the power supply design for each scenario in the 3-Axis Sensing signal chain option.
The document includes the power requirements, the block diagram and power tree, and the recommended…