Hello
I want to contol ADF4360-3 using NI myRIO (datasheet)
I have the eavluation board EV-ADF4360-3EB1Z for this Integrated Integer-N Synthesizer and VCO.
can any one help me in this regard...
Hello
I want to contol ADF4360-3 using NI myRIO (datasheet)
I have the eavluation board EV-ADF4360-3EB1Z for this Integrated Integer-N Synthesizer and VCO.
can any one help me in this regard...
Does anyone know of a way to adjust the frequency of the ADF4360-3 independent of the adjusting the reference, or the counter registers. Perhaps some topology that allows a small adjustment Vtune. The requirement is +/-2kHz or so.
I have the evaluation board of ADF4360-3.
I want to access it using myRIO from National Instruments (NI). This device is Running Linux Real Time OS... If I have the .so library for this device i can access the device using Labview and MyRIO.
this is…
I have used ADI PLL Sim to generate a design for a 900 MHz CW local oscillator using an ADF4360-3. Currently I'm trying to work out how to program into the ADF4360-3 eval board based on the simulation file results. What should the RF output frequency…
I'm observing LO leakage into the inputs (pins 1 & 2 and 15 & 16) of an AD8349 modulator in a direct conversion transmitter (tuned to 942.8 MHz). The analog inputs to the modulator originate from an AD9763 DAC with a low-pass anti-aliasing…
Hello,
I am working on a design with the ADF4360-3 driving a 10W power amplifier through a lattice balun at 900MHz. I have configured the registers to output ~900MHz and the loop locks when the PA is not powered. Spectrum analyzer confirms the correct…
I received this customer question:
I have a question regarding the ADF9360-X series PLLs. In the datasheet for these devices It is stated that three bytes should be sent via SPI to configure the different registers on the device. When I send three bytes…
Hi
first of all : excellent forum, nearly all of my questions solved by reading some posts. Good search function.
Now the situation and question:
1)
In our design we need a receiver LO frequency around 1100 MHz. Phase noise requirements are nearly…
Ihave the evaluation board for ADF4360-3 ..
i am trying it to control using myRIO and LabVIEW from national instruments (NI). myRIO uses Linux Real time OS..
i can access shared object using LabVIEW...
can you help me to access the evaluation board…
I have a board with a ADF4360 on it (see pic below). At the moment I haven't been able to get any output from it. I wouldn't class myself as an expert in RF things so any tips would be appreciated. At the moment the output inductors L1, 2, 3 are not fitted…