• Can the initialized ADF4360-1 disconnect from PC

    Hi,

    I am currently undertaking a project that requires an independent 2.4GHz frequency synthesizer.

    ADF4360-1 is a good choice and many people use a microcontroller to initialise the IC.

    Regarding to its evaluation board, the initializing procedure…

  • ADF4360-1制作和测量问题

    ADF4360-1我按照正常的步骤做了,画的PCB,然后测出来的结果是输出-30dBm,中心频率在2.34GHz,请问这是为什么啊,是射频线阻抗没设置好吗?(我板厚度1.6mm,用的FR4板子,程序控制的中心频率是2.4Ghz,-6dBm输出)

  • ADF4360-1 Evaluation Board software problem

    I currently purchased adf 4360-1 evaluation board and want it to generate a output of single frequency at 2310 MHz at output power level varying from -3dBm to-12dBm.

    I saw that there are lot more options in the software interface:

    PFD frequency

  • 关于ADF4360-1/2使用疑问

    1、参考时钟REFin输入采用方波输入时:

    1)交流耦合还是直流耦合?

    2)采用3.3Vcmos方波输入电平时,是直接直流耦合输入还是交流耦合?手册中的输入口推荐电路该如何理解

    2、供电

    Vvco管脚的供电是否需要和VDD、AVDD供电分开,是否可以合用?

  • how to generate 1.5-30MHz with 1 MHa step size using adf4360-9?

    how to generate 1.5-30MHz with 1 MHa step size using adf4360-9?

    suggest

    L1 and L2 values to cover band.

  • RE: ADF4360

    To avoid pick-up it might be a very good idea to use the ADF4360-1 with divide by two enabled.

    If your system can handle the extra power consumption, the ADF4351 would also be a good option, as this permits divide by 4 at the output.

  • ADF4360-x software

    The latest ADF4360-x software is attached. This is compatible with all the ADF4360 family.

    Installation process:

    1. Disconnect any evaluation board

    2. Download and run the attached installer

    3. Click Next/Continue/Finish when asked

    4. Connect your…

  • RE: ADF4360-8 driving AD9268 problem

    Hello Michael,

    Can you take a spectral plot of the RF output of the ADF4360-8...1) narrow band , and 2) wide band to show what spurs are present .

    regards,

    Brigid.

  • ADF4360 Evaluation Board Control Software

    The latest ADF4360-x software is attached.

    Installation process:

    1. Disconnect any evaluation board

    2. Download and run the attached installer

    3. Click Next/Continue/Finish when asked

    4. Connect your evaluation board

    5. Windows will detect the evaluation…

  • Adf4360-0

    First of all thank you very much for your excellent forum, I'm doing a  Design of an Economical Antenna-Gain and Radiation-Pattern Measurement System, for that I dispose of a adf4360 and AD8302 detector, my problem is with adf4360 when checking the…