• ADF4355-2 Frequency Update Sequence

    Hi, 

    I would like to ask some questions regarding the ADF4355-2. Currently I am able to get my expected single output frequency after initialization. However, when i enable the frequency update sequence in my code, the output frequency went haywire.  

    These…

  • RE: ADF4355, ADF4355-2, ADF4355-3, ADF4356, ADF5355, and ADF5356 evaluation board control software

    Would you please send me the source code as well for the ADF4355-3 eval GUI?

    Thank you.

  • ADF4355-2 can not work normally

    I’m configuring ADF4355-2 with a phase detection frequency of 25MHz, and using MUXOUT shows that the R frequency division is correct, but in any case, using MUXOUT to display the N frequency division is a fixed value of 20MHz, CPout and Vtune are always…

  • ADF4355-2 output synchronization

    Hi All,

    We want to use ADF4355-2 to generate LO for Demodulator and modulator at the same time.

    System RF output frequency maybe will at 3GHz to 4GHz.

    We have some question as below need your help!

    1. Does ADF4355-2 use RF outputA and B at the same time…
  • ADF4355-2 PLL phase issue

    Hi All,

    We want to use ADF4355-2 to generate LO for Demodulator and modulator at the same time.

    System RF output frequency maybe will at 3GHz to 4GHz.

    We have some question as below need your help!

    1. Does ADF4355-2 use RF outputA and B at the same time…
  • ADF4355-2

    Hi! I would like to ask if anyone has details for ADISIMPLL or ref file using ADF4355-2? Especially with loop filter and settings used from datasheet? Thanks.

  • ADF4355-2 and ADF5355 Evaluation Board User Guides (Preliminary)

    Attached are the user guides for the ADF5355 and ADF4355-2 evaluation boards.

    It is important to note that these user guides are preliminary versions, and hence are subject to alteration.

    Update: EV-ADF5355SD1Z user guide on Analog.com: http://www.analog…

  • ADF4355-2 θjc

    Hi,

    θjc of ADF4355-2BCPZ(32-Lead LFCSP) is available ?

    Best regards,
    Makio