Board 1: VCO output can be locked by adjusting the current value of loop filter and Icp…
Board 1: VCO output can be locked by adjusting the current value of loop filter and Icp…
Is it possible to achieve phase consistency between two
ADF4159/ADF4169 PLLs ?
Two ADF4156 PLLs can be programmed to achieve phase consistency, in the datasheet this is explained in the PHASE RESYNC section. Unfortunately the ADF4156 does not have any…
With a reference frequency of 112 MHz what level of fractional boundary spurious can I expect to see over the 4 to 8 GHz range? With 112 MHz reference frequency the step size is approximately 3.338 Hz.
Hello,
I'm trying to build PLL synthesizer based on ADF4169 PLL and HMC735 VCO. It's assumed to cover a bandwidth of 1 GHz with center frequency at 11.18 GHz. I've designed the loop filter for this application with LBW 100 kHz using ADIsimPLL. The reference…
Hi,
In datasheet, it is mentioned that, this IC can be used for FSK function.
Can we give external pulse signal to this IC?
Can anyone clarify whether ADF4169 can be used for PWM or not? If not, request to suggest a part which can support PWM.
Hi,
Is the following operation possible using the ADF4169?
[1] The lamp starts in synchronization with the external trigger input. There is zero (or few ns) delay from rising edge of trigger to the lamp start.
[2] Ramp up with 160us. Frequency linearly…
Hi all,
Our customer will plan to design the FMCW radar w/ ADF4169.
Using the function "Delay Between Ramps" and "Fast Ramp Mode" of ADF4169,
can we control like the "Digital Ramp Generator (DRG) of DDS" ?
It is only used…