I wonder what is the Frequency Switching Time of ADF 4156 and what is the max hop rate
Thanks
I wonder what is the Frequency Switching Time of ADF 4156 and what is the max hop rate
Thanks
Hello
Our apologies for the delayed response...
The EV-ADF4156SD1Z board contains the ADF4156 synthesizer, an SMA connector for the output signal, power supplies, a reference oscillator, and an SDP connector. There is also a loop filter (20 kHz) and…
近期使用ADF4156做一款发射机,在搭建PLL电路时,将配置程序写入时,观察MUX管脚(设置N分频输出和R分频输出)都能观察到频率为鉴相频率的周期性脉冲信号,但是VCO的输出频率一直不变,经测试,原因是VCO的输入控制电压一直为0V。使用ADISIMPLL软件进行仿真搭建的三阶无源环路滤波器,为什么没有将电荷泵的信号积分为要控制VCO的电压(2V左右)?另外,配置完毕MUX管脚(设置N分频输出和R分频输出)波形正确是不是说明晶振和配置程序都没问题?还应该怎么调试?弄了好久,请各位大侠解决
附件1为ADISIMPLL仿真文件…
您好,
关于ADF5001和ADF4156的连接,参考设计上给的是最好用差分线来连接,但是没有给出如何详细的布设这一差分线,感觉这个应该比较重要,不知到有没有详细的参考设计图?我是个新手,对这个还不是太清楚,根据我的理解ADF5001差分输出阻抗是100欧,那在pcb板上如果使用微带线的话,对应于RFout - RFinA,和RFOUT_N - RFinB的微带线特征阻抗是不是应该设计成50欧,还有这个连接需不需要终端匹配? 如果需要的话应该如何进行匹配?
还请大牛们给予帮助,谢谢!
Hello!
I've been using ADF4156 to design Local Oscillators at frequencies in the range of 5 to 6 GHz.
I use ADISimPLL and Fraction N software for the design.
I haven't faced any difficulties in the LO design at the above mentioned frequencies;…
ADF4156 Phase Resync Operation
I am having a problem that the output phase can only keep its relation to
the ref phase for about one minute after phase resync operation. How can I
make sure the phase relation is matched all the time? I followed the
calculation…
Is it possible to achieve phase consistency between two
ADF4159/ADF4169 PLLs ?
Two ADF4156 PLLs can be programmed to achieve phase consistency, in the datasheet this is explained in the PHASE RESYNC section. Unfortunately the ADF4156 does not have any…
Hi Payam,
The circuit described in Figure 3 of CN0174 consists of several PC boards connected together.
We do not have complete schematics for the entire system, but we do have documentation for the individual evaluation boards for the ADF4156 and the…
Hi!
Let me join your discussion. I have similar problem with my ADF4156 chip. It sometimes locks to a wrong frequency. I try to make a periodic frequency modulated signal of two (close enough) RF frequencies. Each frequency step period is around 20us…