• ADE9153A ACTIVE ENERGY CALCULATION

    Hi Team, 

    I can't find the active energy calculation in ADE9153A but only available for ADE7953 (page 26). 

    Want to understand that can ADE9153A to use for this calculation? If yes, please guide. 

    Thanks. 

      

  • ADE9153A/ADE9153B Comparison

    Hello,

    We would like to know the differences between ADE9153A and ADE9153B.

    Thanks and regards

  • ADE9153a angle

    Dear sir,

    if i using the channel B only, so i can't measuement the angle??

    due to the datasheet show, angle measurement channel A is necessary

  • ADE9153A CF1/CF2 Programming LED for Pulse

    Hi,

    ADE9153A - How can I program a pulse output that generates exact 1600 pulses at 1KWh active power ? 
    Can the number of pulses be calculated ?
  • ADE9153a Guard trace

    I have a question about the layout guidleines for the ADE9153a:

    Is the guard trace from VAMS to VAN under the package necessary due to safety reasons or performance reasons? 

    Because we're having issues with the layout with it, but our accuracy demands…

  • RE: ADE9153A checksum Algorithm using in UART,

    Any update on this? I would like to know as well 

  • ADE9153A DESIGN HELP

    I am designing an energy metering circuit using ADE9153A for 32A charging station. I prefer CT (2500:1) for phase current measurement. But I am having issues

    1) Can I use a CT in  the current channel B to measure phase current?

    2)How to connect IBMS pin…

  • ADE9153A Accuracy Issues

    Hello,

    I'm using the EV-ADE9153ASHIELDZ Evaluation Kit along with the supporting example Arduino code. In addition, I'm also using the equivalent of MTE's PTE 400  to source current to the IAP/IAN inputs and I haven't modified the board at all…

  • RE: ADE9153A UART communication

    Is there any update on this? I also am trying to get it to work over UART. We have prototype boards built and in hand. I am trying to verify communication with the ADE9153A by sending it 0x2420 over UART which should return the Product Version. I get…

  • ADE9153A Burst register values and conversion.

    Hi.
    I am using ADE9153A in SPI mode.

    I am reading register values in burst enable mode from register address 0x0600 which is start of burst register address.

    I need conversion constant for --->  AI_WAV value   and     AV_WAV   value                             

    which are instantaneous…