• Question on ADE7978/ADE7933/ADE7932/ADE7923 devices

    What is the number of harmonics used to calculate the THD?

    Thank you

    Fausto Bartra

  • ADE79xx

    Resources specific to the ADE79xx series of parts can be found here.

  • RE: Need example to connect current transformer to ADE7933

    Hi Fausto,

    I understand better now, I can also suggest the ADE7923, this is a non-isolated version of the ADE7933 with the same footprint and slightly different package (without increased creepage).

    As for connecting the CT, it is very similar to using…

  • RE: Polyphase Energymeter with Total Harmonic distortion

    Hi Panneerajan,

    The ADE7880 is only available in one package, that is the 40-lead LFCSP_WQ.

    The ADE7880 includes, Total Active Energy, Fundamental Active, Fundamental Reactive and Total Harmonic Distortion. It is suitable for use with CT's and has SPI…

  • RE: ADE7878 - Shunt

    Hi Dal-Guy

    It is not possible to use shunt current sensors on all three phases when using a three-phase metering IC such as ADE7878. It is conceptually not possible. The three phase metering IC would have just a single ground potential, whereas while…

  • Range of ADE7978 with ADE7932

    Hi,

    as far as i have understood from searching maximum post on energy meter forum and your product there are only few ics which measure harmonics distortion, one series is ADE7978 with ADE7932/ADE7933/ADE7923 and another is ADE7880. Is it correct

    1…

  • ADI这些器件让传感器充满“智能”,挑战物联网应用so easy~

    谈不完的物联网在人类的日常生活中越来越重要,而随着人类的依赖我们将更多的数据交给云端处理,这样势必会对物联网应用造成“压”迫从而引起更多挑战。包括带宽、处理性能、功耗等方面。

    那么问题来了,怎样做才能应对物联网应用中的挑战?!ADI公司亚太区工业自动化市场高级经理张鹏在ADI年度媒体活动上给出了ADI的解决之道:把一部分处理功能转到传感器这端,让传感器也充满“智慧”,问题便迎刃而解——网络只需传递经过预处理的精简数据,实时性要求强的智慧功能已在传感器端处理完毕,功耗也随之分散到了物联网络的各个部分…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…